VM.START

Description

VM.START starts program execution. Or if program execution was stopped with VM.STOP, VM.STARTstarts the program at the point it was stopped.


  • This keyword is executed when the continue icon is pressed in the Program view.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1156

No Command No

M_01-05-11-000

Related Topics

VM.STOP | VM.RESTART